Other Parts Discussed in Thread: LDC1101
Hi
May I please ask for some expert advice before I go and break my back trying? I have numbered the questions in priority order.
1. Would it work to connect a variable reluctance sensor as the "coil" to one of your LDCs? (I have already ordered the LDC1314EVM))
Background to question:
In applications when variable reluctance (VR) sensors are used for sensing speed or position the main disadvantage is that they will not work at low speeds or with large air gaps. The problem with these sensors is that:
a) They need to be mounted very close to the pole wheel (small air gap)
b) They do not give any signal at low speeds.
My hope is that one could use one of your LDC to detect the teeth of a tooth wheel (presence of a metal teeth or not).
VR sensor basic data
I made some measurements (with a multimeter) of our VR sensors and the inductance is approx 880mH and this change approx 2-10mH when the tooth is there or not. The temperature of the sensor may in extrem cases vary between -40degC to 150 degC so the resistance will change accordingly.
More questions
2. Will the LDC survive the induced voltage when the tooth wheel starts spinning faster?
3. Actually I would like to be able to detect the temperature as well so perhaps a LDC capable to measure resistance could be used?
4. Could you please advice of what settings and components to use?
Thanks in advance!