This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1314DIAL-EVM: Sensing Solutions EVM GUI- does this work with LDC1314DIAL?

Part Number: LDC1314DIAL-EVM
Other Parts Discussed in Thread: TIDA-00508

The installer TIDA-00508 GUI & FW Installer 1.0  doesn't install the Gui app. I run as administrator with virus scan turned off, I get error " Cannot complete the Device Driver  Installation wizard". Should I see COM ports in device manager? Please Advice. Thank you.

  • Hello,
    Have you tried installing on a different computer? Also, what version of Windows are you using? We have fully validated the installed with Windows 7. After installation, the root directory is typically located in the following location:

    C:\Program Files (x86)\Texas Instruments\TIDA-00508 Inductive Dial-1.0

    Please confirm that this directory exists. If it does, but he driver is not successful during installation, then you may have to install manually. The driver is be located in the following: 

    C:\Program Files (x86)\Texas Instruments\TIDA-00508 Inductive Dial-1.0\EVM Driver

    The board should show up in the device manager under the COM port. 

    Regards,
    Luke