Hello,
I'm evaluating LDC1614 for a metal object sensing application in automotive industry. For our application, we are not interested in precise inductance measurements. It is more or less a proximity detection application.
I'm currently reading the sensor output from the LDC1614 EVM and developing the required algorithms. However, during the tests I noticed that the output data is always contaminated with impulses. I cannot determine the reason for these random high peaks which are not sustained but repeated.
I plotted the output in excel to make things clear. Please find following two graphs.
Graph1:
Graph 2:
Graph 2 has the required waveform. As you can see, the graph 1 is contaminated with high amplitude noise signals.
I have implemented a software filter to remove the impulses. However, it would be comforting to know the reason for those impulses and any input from the experts would be appreciated.
Thanks!