Good afternoon friends!
I recently asked a question on the forum about detecting small particles. Unfortunately, as I was told, there is currently no information on what particles are able to uncover the LDC. It is necessary to compensate for this knowledge gap.
All the same, I want to understand this. We know that the LDTS1101 has some limitations in the construction of the sensor (the frequency should be from 500 kHz to 10 MHz, Q-factor from 10 to 400, etc.). Question: what parameters of the coil should be to detect the smallest particles?
I understand that the frequency needs to be increased (in order to achieve large losses in the eddy currents in the target), it may still be necessary to strive for greater inductance and lower capacitance, because the magnetic field in this case will be greater) ??
Or some more tips / comments?