Part Number: BQ24133
Other Parts Discussed in Thread: , BQ24610
Hello team,
I am supporting an application using BQ24133, the project will have a 2S1P Lithium-Ion battery and has a voltage source of 9.0 V, the guide for the evaluation module (BQ24133EVM-715-15V) mentions that the supply for charging needs to be at least 1.0 V above the maximum battery voltage (which would be 8.4 V in this case), but I couldn't find the same mention on the BQ24133 datasheet.
Q: Is it possible to use a 9.0 V source to charge a 2S1P Li-Ion battery to maximum charge (8.4 V)?
Q: If so, What design considerations should be taken?