This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443: How to create a CSS project for IWR1443 and How to create a CSS project for Complie and Debug the MMW Demo for IWR1443

Part Number: IWR1443

Tool/software: Code Composer Studio

Dear engineer!

I wanta know 

How to create a CSS project for IWR1443   and   How to create a CSS project for Complie and Debug the MMW Demo for IWR1443



 thank u so much!

  • Hello,

    You can use one of your Demo projects from mmWave SDK installation directory and start by duplicating the folder for demo

    After doing so you could reuse the compile scripts available vis SDK infrastructure. Please make sure all the prerequisites mentioned in the SDK's documents.

    Alternatively you can find a download and compile CCS project for demo via following link:

    Download and build the mmWave SDK EVM Out-of-Box Demo source code

    Above link is available under mmWave SDK EVM Out-of-Box Demo Training.

    Thank you,

    Vaibhav

  • Hi Allen,

    Both options Vaibhav mentioned are valid. I think the simplest way to create a full CCS project which you are able to compile in one click, is to follow the link Vaibhav provided to download and build the out of box demo. Navigate to Software -> mmWave Training -> Demos -> mmWave SDK Demo as shown in the screenshot below. The setup guide here outlines all the steps you would need to follow to import the project and build it.

    Regards,
    Kevin