This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Implementing the RADAR in Physical environment

Part Number: AWR1642


Hi all,

I am able to connect the AWR1642 BOOST to my PC and run the visualizer on TI cloud platform and find the detected objects on the plot. Now I intent to implement Adaptive Cruise control system. In orde to do it, I just want to use the front 30 degrees as the field of view and consider the objects only within it. How could I access the values of the 2-D points of the objects detected? One method is to use the javascript file of the Visualizer to access the values that are sent for plotting . Is there Any other way through a C/C++ program ? I just want to access the values.  

Thanks 

  • Hello Amol,

    For data format of Out of Box demo.
    The function MmwDemo_transmitProcessedOutput is touched upon in html help:

    file:///C:/ti/mmwave_sdk_01_00_00_05/packages/ti/demo/xwr14xx/mmw/docs/doxygen/html/main_8c.html#ac3a90335aea273ffb5d4cc76d780a55d

    Transmits detection data over UART.

    The following data is transmitted:

    Header (size = 32bytes), including "Magic word", (size = 8 bytes) and icluding the number of TLV items TLV Items:
    If detectedObjects flag is set, pbjOut structure containing range, doppler, and X,Y,Z location for detected objects, size = sizeof(objOut_t) * number of detected objects
    If logMagRange flag is set, rangeProfile, size = number of range bins * sizeof(uint16_t)
    If noiseProfile flag is set, noiseProfile, size = number of range bins * sizeof(uint16_t)
    If rangeAzimuthHeatMap flag is set, the zero Doppler column of the range cubed matrix, size = number of Rx Azimuth virtual antennas * number of chirps per frame * sizeof(uint32_t)
    If rangeDopplerHeatMap flag is set, the log magnitude range-Doppler matrix, size = number of range bins * number of Doppler bins * sizeof(uint16_t)
    If statsInfo flag is set, the stats information

    Parameters
    Please see if this information helps you obtain the required data structure information.
    Thank you,
    Vaibhav
  • Hi Vaibhav,
    Thank you for the reply. However, I could not find the similar documentation for the xwr16xx directory as that is the one I am concerned with while using the AWR1642 BOOST.
  • Hello Amol,
    for AWR1642 you can look at the following doxygen : file:///D:/TI/MMWAVE_SDK_v01.00.00.05/packages/ti/demo/xwr16xx/mmw/docs/doxygen/html/index.html
    Look at the output format sent to host and list of detected objects section.

    Regards,
    Vivek