This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Radar Sudio: HSDC Pro V4.7

Part Number: AWR1642BOOST


Hi Experts,

I am using Rader Studio V1.7.4.0 with HSDC Pro V4.5 and this system works correctly.
Our customer informed us that now HSDC Pro V4.7 was available and it was installed.
According to him, with HSDC Pro V4.7, it asks "No firmware, Please select a device to load firmware into the board." again and again.

Procedure :
  1. HSDC Pro V4.7 run.
  2. "No firmware. Pease select a device to load firmware into the board."  --> OK
  3.  Select AWR16xx_lvds_4Channel....... in HSDC Pro GUI.
  4.  "Do you want to update the Firmware for ADC?" --> Yes
  5.  "No firmware. Pease select a device to load firmware into the board."  is shown again.

I have not tested it yet, but it seems V4.7 does not work.

If somebody conirmed that it works with V4.7, please let me know.
Best regards,
Hitoshi