Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1642BOOST
Hello all,
Could you help me with the following request please,
We are working on industrial safety applications and we want to employ your low cost MIMO sensor in our applications field. Accordingly, I want to buy one of the hardware either IWR1443BOOST or IWR1642BOOST and I have some questions regarding both. Personally I couldn't decide, so I will mention my application area and I hope I get a recommendation from your side.
1. I want to measure Micro-Doppler’s, so I think fast chirps and high sending rate is required as I will need large number of chirps per measurement. Moreover, a suitable maximum range is needed, so a large number of samples per chirp are also required. So, please recommend as I couldn't decide one with radar hardware accelerator and one with built in DSP and I want to decide which is most suitable for the application, given I manly program everything on the PC as a prototype. However, the most important thing for me is ((real-time)) data access and processing.
2. In the boost is everything all included in the package or I have to buy the chip and the boost alone?
3. Is the chip PC communication protocol available with the chip, so that I can develop my own interface in whatever language I want?
Thank you in advance.