Part Number: IWR1443BOOST
Hi,
In our medical device development project we would like to use the IWR1443BOOST for accurate short range (from 5cm to 30cm) distance measurement with a resolution around 0.1 mm.
As I understand at this point, just by relying on the frequency shift of the IF-signal using the 4GHz max Bandwidth of the device the max resolution is only around 5 cm (as observed with the drone altitude demo and calculated with the "mmWave Sensing Estimator"). However using the phase of the IF-signal it should be possible to reach sub-millimeter accuracy (vital signs demo). On the other hand, in all examples I found that the phase-based distance measurement was only used in the context of vibrating/periodically moving objects (water surface, engine, heart beat, etc).
In our case we would like to measure an object moving on the mentioned very short range (25cm) with high (0.1mm) resolution. We would like to have this fine resolution on the full range. As an example: the object can be 70.4mm away from the sensor and it can move to a position which is 125.7mm away from the radar and just stay there. So the motion of the object is not periodic at at!
Is it possible to configure the device to achieve the above mentioned goal? If yes how to do it? (Basically we want to substitute a laser distance gauge with this radar).
Thank you in advance,
Viktor Varjas