Other Parts Discussed in Thread: AWR1443, UNIFLASH, ,
Hi,
What's the difference when select AWR1243 or AWR1443 in Uniflash to burn the spi flash?
I have one AR1243 ES1.0 EVM and I tried to burn the bss/mss binary (DFP 0.6 version) on spi flash, then to use Radar studio v1.7.4. And I got below result.
1. Using Uniflash to flash the spi flash by selecting AWR1243. Then it is ok to connect SPI in radar studio, but RF power up time out.
1. Using Uniflash to flash the spi flash by selecting AWR1443. Then it is ok to connect SPI in radar studio, but RF power up ok and following configures in radar studio all work ok.
So I think there should be some difference when using Uniflash to burn spi flash. Would you pls kindly advise? The reason I asked the question is that customer uses radar studio to burn the spi flash on their own AWR1243 ES1.0 board and met RF power up time out issue when using radar studio.