Part Number: IWR1642BOOST
Other Parts Discussed in Thread: MATHLIB
Tool/software: Code Composer Studio
Hi,
I am having problems verifying my installation of Code Composer Studio 7.3.0. After installing CCS and the mmWave SDK, I am able to import the mmw and mmw_dss examples from the resource explorer, and building the mmw lab example works.
When I try to build the mmw_dss project, I get the following error and am not sure what to do to fix it.
Error:
>> Compilation failure
subdir_rules.mk:21: recipe for target 'dss_main.oe674' failed
"../dss_main.c", line 85: fatal error #1965: cannot open source file "ti/mathlib/mathlib.h"
1 catastrophic error detected in the compilation of "../dss_main.c".
Compilation terminated.
I am running CCS on Ubuntu 16.04. The mathlib_c674x_3_1_2_1 folder has been installed with the SDK and located in the CCS installation folder.
Is this a permission problem or maybe files stored in the wrong location? Any suggestions are much appreciated.