Other Parts Discussed in Thread: AWR1642
Hi
I managed to capture some binary files using Radar Studio & High Speed Data Converter Pro (using AWR1642BOOST,MMWAVE-DEVPACK, and TSW1400 hardware).
Post processing using Radar Studio works fine. I now need to do some manual processing in MATLAB, so i import/open the binary in MATLAB
fileID = fopen('adc_data.bin'); A = fread(fileID);
whos A in MATLAB is returning:
Name Size Bytes Class Attributes
A 16711680x1 133693440 double
Now when i had a look at the data, it seems to be 8 bit (value ranges from 0-255) instead of the expected 16 bits (0-65535). i believe the data are 16 bit (and yes, in HSDC Pro i did load the corresponding 16 bit firmware , not the 14 or 12 one). In "Codes" and "Bits" View of the waveform it's definitely 16 bits.
Importing it as a 'uint16' seems to fixed the issue.
Could you please confirm this?
Thanks