Other Parts Discussed in Thread: MMWAVE-SDK, UNIFLASH
How can I switch to a Contiuous Tx mode (frequency modulation off) in AWR1443BOOST ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How can I switch to a Contiuous Tx mode (frequency modulation off) in AWR1443BOOST ?
Hello,
I tried loading the below config from the location which was pointed out but didn't get any measurable output power (equipment noise floor is -30dBm)
% ********************************************************************
% * Sample DEMO Script
% ********************************************************************
flushCfg
dfeDataOutputMode 2
channelCfg 2 1 0
adcCfg 2 2
adcbufCfg 0 0 1 1
lowPower 0 0
contModeCfg 77 0 0 8000 0 0 30 1 1024
setHSI LVDS ADC disable
sensorStart
However, the below script enables FMCW modulation and gives a measurable output power (>-7dBm)
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 2 1 0
adcCfg 2 1
adcbufCfg 0 1 0 1
profileCfg 0 77 921 7 114.29 0 0 35 1 224 2107 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 0
frameCfg 0 0 32 0 33.333 1 0
guiMonitor 1 1 0 0 0 1
cfarCfg 0 2 8 4 3 0 1280
peakGrouping 1 1 1 1 229
multiObjBeamForming 1 0.5
calibDcRangeSig 0 -5 8 256
sensorStart
Can you help check if the Con_Tx script needs any change? Also, I'm using AWR1443BOOST, do I need any jumper/device-pack change?
Regards,
Ashish
Hello Vivek,
I'm getting an error (Missing command profileCfg). In dfeDataOutputMode 2 , there should be not a need for profileCfg.
contModeCfg should have been sufficient. Below are the steps and scripts followed:
Below are the steps I followed