Hi,
Human when moving is identified but unable to detect human when static using the SDK1.05, human is with in 15Meters range.
Following are the configuration settings:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Human when moving is identified but unable to detect human when static using the SDK1.05, human is with in 15Meters range.
Following are the configuration settings:
Hi Maruthi,
If you are interested in the problem of 'people detection' using radar, I would suggest looking at the people counting reference design ().
I would also suggest that you move to SDK 1.1, as it has an additional feature (called clutter removal) that would help with nearly stationary objects (like people).
If you would like understand as to why people are not detected using your current configuration, you can collect ADC data of a single frame and process it offline to see why detections are not occuring. You might discover that the clutter in the scene is too dominant, or that the SNR requirement (for CFAR) is too high.
Regards
Anil
Hi Maruthi,
One thing you can do (as a temporary measure) is to check the 1D profile in the Radar Visualizer. Enable the option for 1D profile and see if the target (in this case a person is visible).
You can then reduce the CFAR threshold until the person is visible. You can try the modified configuration given below.
Regards
Anil