Other Parts Discussed in Thread: IWR1642, , IWR1443
I bought the IWR1443BOOST dev board and have been using it. I have read a ton of different manuals and have run through the demos and I understand some of it, but not enough that I can confidently modify the existing examples to work as a prototype sub-component for a new application. I would like to have multiple sensors, either IWR1443 or IWR1642 based, connect via SPI, UART, I2C or some other low-level interface to an FPGA and NOT use a microcontroller (or an RTOS). All of the demo projects I can find use an RTOS and TI microcontroller. Is there info available that describes how to design with this IC at a lower level, using just the IC itself?