Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642
Hi,
I am facing a specific problem with data capture & analysis using AWR1642. The scenario has a high RCS Corner Reflector at around 1.5m (10th bin in Range FFT). This is identified as a very large peak at the same distance after taking Range FFT. My problem is, There is a small reflection at the higher range also. Considering that I have 256 range bins, I see a small peak in the FFT result at 245th bin (255-10). This reflected peak does move when I move my Corner reflector.
I call it as small peak because the amplitude value is very small compared to the Corner reflector but considering its surrounding area, the peak is significant and gets detected at CFAR.
The peak disappears when the Corner reflector is moved away from the sensor by more than 3m. As long as the reflector is within 3m, the corresponding (255-actual bin distance)th bin has a peak.
This problem is seen in the ADC dump captured using AWR1642EVM on analyzing it in Matlab.
I would like to know the reason for this reflection of high RCS object. And Any solution to avoid this.
Thanks in Advance
Santhana Raj