Part Number: IWR1642
Hello, TI employees.
I am trying to redesign the antenna configuration of IWR1642Boost in order to measure the elevation and azimuth angles simultaneously using IWR1642 chip.
To this end, I moved one tx antenna element vertically by lambda/2. I initially thought using BPM MIMO technique can measure much higher velocity than TDM MIMO.
Because shorter the chirp duration, higher the maximum velocity. In TDM, chirp duration cannot be shorter than 2Tc, where Tc is the shortest chirp duration that IWR1642 can work.
If what I know is wrong, please correct me.
In BPM MIMO, decoding with 2 Tx, 4 Rx is performed during 2 chirp intervals S1 = Sa + Sb, S2 = Sa - Sb, where Sa = S1 + S2 received during t0, Sb = S1 - S2 received during t1.
And Tx1 transmits S1 Tx2 transmits S2 at every interval.
I have question from here. I think S1 at t0 and S1 at t1 are different with an object with a high velocity.
I think the above equations S1=Sa+Sb and S2=Sa-Sb assume that the phase difference of two intervals t0 and t1 is zero. Am I right?
If I am right, I think the maximum velocity when using BPM MIMO technique is limited to a certain value.
Do we have no difference between using BPM and TDM MIMOs? Which one have better maximum velocity?
Please let know the better solution for measuring the higher velocity with simultaneous elevation and azimuth angles.
Thanks.