Hi,
I found two formulas to calculate Doppler resolution.
One is in mmWave.js: P.dataPath[idx].dopplerResolutionMps = 3e8 / (2*P.profileCfg[profileCfgIdx].startFreq*1e9 *
(P.profileCfg[profileCfgIdx].idleTime + P.profileCfg[profileCfgIdx].rampEndTime) *
1e-6 * P.dataPath[idx].numChirpsPerFrame);
I think chirp rate = 1/(idle time+rampEndTime)
As Number of DopplerBins = Number of ChirpsPerFrame / Number of TX antennas, if number of TX antennas is not 1, the chirpsPerframe is not equal to the number of dopplerbins. That is, when no. of TX is not 1, these two formula will output different result.
Which one is correct? Or does I miss anything?