Tool/software: Code Composer Studio
HI
i'm calling the mmwave api as below and wish to get the monitoing report :
rlRxNoiseMonConf_t rxNoiseMoncfg; void MmwDemo_mssInitTask(void){ ...... rxNoiseMoncfg.profileIndex = 0; rxNoiseMoncfg.reportMode = 0; //check periodic without threshold rxNoiseMoncfg.noiseThresh = 250; rxNoiseMoncfg.rfFreqBitMask = 1; //check the center retval = rlRfRxNoiseMonConfig(RL_DEVICE_MAP_INTERNAL_BSS,(rlRxNoiseMonConf_t*)&rxNoiseMoncfg); if(retVal!=0){ system_printf("error"); return -1; } system_printf("finished rx noise monitoring configurations into bss\n"); ...... }
after that i check the bss async event in the function MmwDemo_mssMmwaveEventCallbackFxn(uint16_t msgId , uint16 sbId, uint16_t sbLen, uint8_t *payload)
i can recive the msgId = 80;(PL_RF_ASYNC_EVENT_MSG)
but i can never recive the asyncSB for RL_RF_AE_MON_RX_NOISE_FIG_REPORT.
did i miss something or make some mistake?
please help to check that .
br
havi