Other Parts Discussed in Thread: AWR1642BOOST, AWR1642
Issues with DCA1000EVM Data Capture Card attached to AWR1642BOOST
July 18, 2018
I bought an AWR1642BOOST version 2.0 that seems to work as advertised with mmWave Demo software running on a Windows10 computer.
Then I bought a DCA1000EVM and am having problems working through the DCA1000EVM Quick Start Guide
First I list a series of questions keyed to an attempt to follow the "DCA1000EVM Quick Start Guide" (SPRUIK7-May 2018).
Then I present gory details on what I tried.
QUESTION 1: When I installed mmwave studio (Quick Start step 4 below) the installation seemed to go OK (windows with bars moving, etc.).
However it was not clear how to run the program. Many folders with files were installed to a folder named
C:\ti\mmwave_studio_01_00_00_00.
After some looking I found a file named C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\RunTime\mmWaveStudio (Application).
When I ran this application file I got the display screen shown on the "Quick Start, section 1 getting started" page2
but there was one minor difference, the RED “DCA1000” at the upper left corner above “RadarAPI” is missing
I assume this is the right program to run. AM I CORRECT SO FAR??????
QUESTION 2: When I click "Set UP DCA1000" on the left side of the screen I get a window labeled "RF DataCaptureCard".
At any point in step 7 or 8 (see below) this window displays "FPGA version: 0.0.0.0" (see NOTE1 below)
Is this a hint that something is wrong in the DCA1000 FPGA firmware?
If so, do you have any suggestions of what is wrong or what to do about it?
QUESTION 3: See problems at step 8 below. What location should MSVCR120.dll be stored in (assuming that is my problem)?
QUESTION 4: In mmWave Studio GUI user’s guide, section 9.3 is a note “2. Matlab Run Time Engine (Version 8.5.1) and
HSDCPro Software are pre-requisites for Post Processing utility available in mmWaveStudio GUI”.
Do I need these software installed or running at this time? If not, when do I need it running and can you point me to some documentation?
IHDSC Pro didn’t install to the same directory as mmWave Studio. Is this a problem? If so, what needs to be done.
DETAILS FOLLOW:
Items numbered below correspond to numbering in the "DCA1000EVM Quick Start Guide"
They were accomplished apparently successfully except when noted:
1. Attached boards physically as shown in Figure 1 of Quick Start Guide
2. Data and Supply Cable Connections:
a. Micro USB to J1 on DCA1000 for FTDI interface
b. Micro USB to J8 on AWR EVM for XDS110 interface
c. Ethernet RJ45 cable to J6 on DCA1000
d. Two 5V 3A power supplies, one for each board
e. Jumpers on SOP0 and SOP1 (development mode)
f. SW3 switch set to DC_JACK_5V_IN
3. Static IP address for computer set as shown in Figure 3 and no other devices on Ethernet
4. Download and install the mmWave Studio and the Matlab Runtime Engine
5. Installed the FTD drivers
6. Ports are as shown in Figure 4 except, as expected, the numbers assigned to COM ports are different.
7. At this point I ran mmwave_studio to get the display needed to “Issue a board reset and connect the RS232 COM port”
required in this step of the instructions. Running the program I see FTDI connected and if I click on the reset button
a yellow LED on the AWR1642 board blinks. If I set the proper com port and baud rate in the RS232 window and click on connect,
RS232 status shows green (connected).
8. At this point, I selected the file DataCaptureDemo_xWR.lua and clicked run. Everything seemed to run correctly at first;
the proper lines in the upper middle were filled out (green when appropriate), the BSS and MSS firmware was loaded,
SPI Connected, and RF Powered-up.
But then in a few seconds an error message box popped up saying “Packet_Reorder_ZeroFill.exe – system error” “code execution can’t proceed
because MSVCR120.dll was not found”. I tried reinstalling the Mmwave Studio again with the same results.
The last two lines in the output window were:
[Radar API] : Packet Reorder Utility Started … please wait ….
[Radar API]: arl.PacketReorderZeroFill (“ then a bunch of file names “)
ADDED NOTES
NOTE1: Following the "mmWave Studio GUI user's guide" Figure 9.3 shows FPGA Version: 2.5 Record Bit File but I see FPGA Version: 0.0.0.0.
NOTE2: I have not yet verified that there is ethernet communication between the PC and the DCA1000 using Wireshark as suggested in
"DCA1000EVM Data Capture Card user's guide" section 8, Troubleshooting.
Thanks for any help!!