hello,i use the radarstudio to capture adc raw data,in the 2complex mode, when i set the ADC Samples number under 1024,the result is correct, but when i set the ADC Samples number over 1024, the ADC Samples over the 1024 are 0,when i set the ADC Samples number is 2048,i can not capture any raw data,when i set the ADC Samples number more then 2048 ,the system does not work,i need close the radarstudio and Power on again the awr1243.Can you tell me the reason?radarstudio capture adc raw data.docx