Part Number: IWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH
Hi,
I`m working with mmwaveSDK 01.02.00.05 on IWR1443BOOST (ES2.0) to work Visualizer. I uni-flashed the pre-build Visualizer app binary (located at C:\ti\mmwave_sdk_01_02_00_05\packages\ti\demo\xwr14xx\mmw\xwr14xx_mmw_demo_mss.bin) into the board. Every uni-flash operation seemed to work correctly. But after power cycle without SOP2 jumper, I saw an issue of no responding for the connection in Visualizer. (Visualizer recognized the COM ports correctly with correct baud rates, but never be connected to the target board).
So I switched from Visualizer to TeraTerm to see the raw messages. I asserted reset button on IWR1443BOOST and found the following error returned on the terminal. It seems like having exception error in the application... I think this is the root cause of "no connection" issue, but i`m not sure why this can happen. Could you please suggest ?
Best Regards,
NK