Other Parts Discussed in Thread: OPT9221
1)I might have accidentally deleted/overwrite OPT8241 firmware/software by downloading and installing OPT9221_0v23 and OPT9220_0v27 into OPT8241 using EEPROM Programmer in VoxelViewer 0.7.0. The OPT8241 ToF sensor could not be able to stream after that. Is there any other way to restore back the OPT 8241 ToF sensor software/firmware so that it could start streaming again?? I have tried various way and means such as downloading the FX2-OPT8241 firmware and hardware from www.ti.com/tool/opt8241-cdk-evm , reset the device but to no avail. Is there anyway to reboot/reformat the system back to normal?
2) Is there anyway to change the parameters? I realized that the camera work but couldn't stream due to the parameters after downloading the 2 programmes mentioned above.
3)Do I have to download 3D ToF System estimator tool?
4) I have used the Cypress USB 3.4.7 for its firmware but nothing happened.
I had reviewed other forums but am still feeling very lost and desperately needs help over here!! Thank you in advance!