Dear Sir:
I'm testing the LED current DAC error.But it is different from the datasheet Electrical Characteristics(page11: LED current DAC error ±5%). When I set the current 50mA,This is my test data below.
Module | test current |
0 | 57mA |
1 | 48mA |
2 | 39mA |
3 | 46mA |
4 | 59mA |
5 | 38mA |
For this problem,i have asked your fae,he replied to me:" I got access to the AFE4490 production test data.
The min/max limits for the LED currents are set to +/-25% around the typical value.
From the customer results, looks like they are seeing a +/-20% spread across devices.
So their result seems to be within expected part-to-part variation."
Anyone knows why is it different from the datasheet?
Thanks!