This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900EVM: -/+ 10V output with PGA900

Part Number: PGA900EVM
Other Parts Discussed in Thread: PGA300, PGA900

hello team!

i'm still evaluating pga900 and pga300.. and i have a new question,

if i want a voltage output between -10 and +10 volts with 20000 points of resultion ( that's standard for plc input ), using pga900: i need to add an external circuit or an external dac, and also to generate  -/+ 12V supply. to save space and keep design simple i was thinking about a DAC with 16 bits. best with pwm input.

there is a TI design for this purpose? or any dac IC's that is raccomdend?

thank you very much

best regards

A.F.