Other Parts Discussed in Thread: LM35
The LM 35 datasheet states that the output impedance is about 0.5 ohm but it can only source current (10ma) and that its current sinking capability is limited to 1 uA. Does this mean that while the sensor can easily drive the input to a ADC high it needs a pull down resistor to help it go low? If so are there any guidelines for sizing the pull down resistor?
If the ADC is a delta-sigma design should I also add an external capacitor between the LM35 and the ADC to minimize voltage noise? If so, are there any guidelines for sizing the capacitor?
In both cases, my sample rate is around 10KHz.
thank you
jim