I have essentially the same question as asked back in Feb in this thread "AMC6821: Question of AMC6821 Auto Temperature Fan Control Mode with Remote Channel Not Used" however there was no answer posted to the forum, so the question remains.
We need to use the AMC6821 in automatic mode (FDRC=11) using the *local* sensor only. There is no remote sensor connected.
This automatic mode uses the maximum speed (duty cycle) calculated by the control loops from both the local and remote sensors. How can we configure the device to ignore the remote sensor and use only the local sensor in the control loop calculations?
Thanks -
:: Gavin