Section 2.6 of The SBOA138A article (Easy-to-use cabling interface for measuring temperature with the TMP107) has some recommendations for reducing the voltage drop along the chain.
Since i can get a surface mount capacitor in a 10uF size, which of the following options will be preferrable:
a) Replace my existing 0.1uF capacitors with the 10uF capacitor
b) Add the 10uF capacitor in parallel with the 1uF capacitor. (I am assuming the 1uF will better filter the hgh frequency Vcc ripple than the 10uF so will still be needed)
Thanks
David Nyarko