Read that there was raw data o/p on GPIO3/4
I cannot see this - I am running FW 1.43
Do I need to set anything to enable this?
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Read that there was raw data o/p on GPIO3/4
I cannot see this - I am running FW 1.43
Do I need to set anything to enable this?
Regards.
Yes, you have to select the "Enable UART Stream" option in Debug tab of the GUI. Firmware v1.43 supports UART streaming capability. FYI, there's a later version of GUI and firmware on the web.
thanks, Vishy
Hi Vishy,
I have FW REVISION 2.01, and GUI REVISION 1.2.7.1 and I am trying to get the UART streaming capability enabled. What should the UART settings be for my Hyperterminal interface?
Baud Rate, Parity, Stop and Flow Control? Is it 230400, None, 1 bit, None?
Thanks,
- Russ
Please use 115200, No parity, 1 Stop, No flow control, 8bits.
Thanks,
Vishy
Thanks Vishy,
One more question... is the LabView code interface available? I would like to setup the software to repeatedly trigger the "TDC7200 TOF_ONE_SHOT" button on the LabView GUI. If the GUI is unavailable for editing, how would I go about automatically retriggering the TOF_ONE_SHOT, i.e., at a 200msec update rate? Can you share the command structure being sent to the MSP430 on the TDC1000-GASEVM , so I replicate the "TDC7200 TOF_ONE_SHOT" button press through my own LabView .vi?
Thanks.
- Russ
Russ,
This automatic retriggering function is already available in the GUI through the Graph Tab "START_GRAPH" button. The ONE_SHOT and START_GRAPH commands execute the same code in Firmware. Retriggering happens at the selected "TRIGGER UPDATE FREQ" option in the Setup Tab. You can save data also to a file.
Let me know if you have questions on this.
Thanks,
Vishy