Other Parts Discussed in Thread: TDC1000, TDC7200
Hello,
I currently have the TDC1000-GASEVM and have the registers and everything configured how I would like. I would like to be able to communicate directly with the MSP430 chip on board without using the GUI. By this I mean I would simply like to read the TOF data without using the GUI. Now I am not experienced in firmware/embedded software applications so I am just looking for some information to get me started. I would like to know what I will need to accomplish the task such as software(CCS?) or hardware(cables and the such), maybe some tips on what source code to look at. Also can the firmware be changed directly through the USB connection, or will I need to use the JTAG pins? Is there a benefit to using JTAG?
Also, in the end, I want to be able to send information about TOF over an ethernet connection to a website. Would you recommend staying with the MSP430 for this application, or should I move onto one of the am335x used by the beaglebone black? I mention the am335x in particular because I have a friend who has done a lot of work with it and would help me out if that is the case. Any other suggestions for processors would be appreciated too.
Thanks,
Russell