Part Number: TDC7201
Hello,
Regarding to the application with TDC7201, my customer have a question.
They will design with the following conditions.
・TOF distance : 2000cm(20m)
・TOF durations(start-stop) : 133ns (2000cm+2000cm)/(30cm/ns)= 133.3ns
・Measurement Mode : Mode 1(12 ns to 2000 ns) or Combined mode (0.25 ns to 8 ms)
・TDC7201 fCALIB_CLK : 8MHz
・SPI fSCLK : 20MHz (Host: MPS430)
They will design the performing distance measurement 5000 times per second with above conditions.
Are their designs valid? Is there any problem as total system?
Regards,
Tao2199