Hello,
I am working in the design of the power supply for the TX-SDK-V2/NOPB evaluation module.
In the user guide is mentioned that after the complet power up setup the current draw for +/-50 supply is: "...the ~4mA of current from the +50V supply, ~3mA from the -50V supply...".
In the data sheet of lm96550, the is in the evaluation module, the maximum rating are: 7 mA for VPP and 8 mA for VNN, that are connected to +/- 50V.
I would like to know what specifications must be take in account.
Regards.