Part Number: TDC1000-GASEVM
Hi,
I am using TDC1000-GASEVM with BSTEVM boost circuit. I have interfaced both with Laptop-GUI, but i have not got any output. i interfaced TDC1000-GASEVM with TPS61175EVM, and i got output there. my queries are,
1. Do i need to change any hardware on BSTEVM board in regard to interface with GASEVM?
2. Are there any special register settings for GASEVM board, which should be incorporated while using it with GUI? (apart from TDC1000-HV driver EN 1/2 and TDC1000-HV Boost Power Enable EN)
3. When i checked VDD1 and VDD2 pins on board, i got zero voltage on multi-meter.
4. Here i am using normal transducers from "STEMINC" ( https://www.steminc.com/PZT/en/piezo-ceramic-disc-1-mhz, ) and not gas transducers!
Please help me in resolving above queries!
Thanks,
Rohit