Part Number: TDC1000-TDC7200EVM
I have the same question with other people.
Before I update the firmware, everything is ok and the board can be linked to USB.
Now, I cannot identify 7200EVM through the USB link and also not update the firmware correctly.
ps. I have already use separately "C:\Program Files (x86)\Texas Instruments\TDC1000_7200EVM\MSP430 USB Firmware Upgrade Example" program to upgrade the firmware but still not work.
The message is shown:
Starting
Password Sent Successfully
Sending RAM BSL v00.06.05.34
Done RAM BSL v00.06.05.34
Failed to read data from RAM BSL
Unsuccessful in starting the BSL. Restarting.
Password Sent Successfully
Sending RAM BSL v00.06.05.34
Done RAM BSL v00.06.05.34
Failed to read data from RAM BSL