Hi,
Power supply for LMT85 is rated for (+1.8V to +5.5V) and from the Transfer Table of the datasheet i can see the Vout at -50C is 1955mV~1.9V.
Just trying to understand if I operate the device at 1.8V then also the Transfer table values are valid ? as how i can get the 1.9V output voltage with 1.8V supply voltage.
Or the Transfer table values are specified at a known Vdd say~3.3V.
Please confirm can I use the device without any another voltage reference. My power supply(battery) voltage can vary from 2.7V to 3.6V as I can see there is internal constant current source inside the device.
BR,
Rahul Wagh