Hello,
I am running the fall detection demo on the AOP sensor.
Can I set up more than one static boundary box or more than one presence boundary box?
If it's possible, can I do it via the config file?
Thank you for your help!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am running the fall detection demo on the AOP sensor.
Can I set up more than one static boundary box or more than one presence boundary box?
If it's possible, can I do it via the config file?
Thank you for your help!
Hi,
The fall detection algorithm implemented on top of the 3D_people_count_68xx_demo. The processing of the point cloud to detect the person and detect the fall is implemented as part of the processing in the GUI. Since the implementation was oriented towards tracking one person (for elderly people monitoring use case) only one boundary box is shown.
Based on the reference the same concept can be extended to track more than one person. The implementation can be based on the reference already provided in the 3D people counting demo and GUI example.
Regards,
Sudharshan K N