Other Parts Discussed in Thread: MMWAVE-SDK
Dear team,
currently vitalsign demo mmwave code seems to be stopped inside AOP demo.
I had powered it via raspberry pi 0.
For example, raspberry pi keeps reading buffer nothing once it happens.
It goes fine for more than 2000 number of reading packets in buffer.
and it stops writing data into usb buffer.
I believe that I can set watchdog (sw or hw) when mmwave stop working. So, it can restart when it is stalled.
Question 1. how to restart or reset mmwave without unplugging and plugging usb ? ( I had powered only via usb from rasp 0)
Question 2. are there any setting for watchdog system(DWD in BIST) when it is stalled? any example?
BR,
kisub