Other Parts Discussed in Thread: AWR6843, AWR6843ISK
Short description: AWR6843AOPEVM technical inquiries.
Application : Automotive : Passenger Vital Signs detection and monitoring.
Below, the questions :
- Is it possible to change the heart rate bandwidth [0.8,2HZ] to higher frequencies?
- Is there an adequate configuration for "in vibration uses" ? (Automotive application)
- The FOV of the sensor is 120° H & 120° V, is it defined by design ? or could be changed via SW configuration?
- The calibration process is started at start-up; it is noted that it lasts between 15 and 20 seconds but has been found to take longer for the values to stabilize.
What functions are established during calibration? - Could i change the calibration parameters without changing the EVM FW?
- We noticed that the sensor heats up a lot. Does this influence the processing of the data and the measurements acquired?