Part Number: LDC1612EVM
Hi,
I am using the LDC1612EVM for linear sensing application.
The coil being used has the following parameters attached below:
The sensor inductance sampled value has a baseline at 58uH and raw data value of 6413055.
Frequency set at 3.3MHz .
I was expecting the baseline inductance to be at 7.5uH in the graph and increase/decrease according to the target movement.
Also I was expecting the raw data to be starting from 0.
Kindly help.
Thanks