Other Parts Discussed in Thread: DRV5032, TMAG5170
I would like to inquire about a digital hall effect sensor:
Our company designs and manufactures an IOT water flow system. We are currently using in our design your DRV5012 and its working well for us.
However, since we are replacing our mechanical design, we require a sensor that will have a through hole package such as TO-92.
We were unable to find in TI’s portfolio a sensor with a through hole package, that will have the low power properties of the DRV5012(down to 1.3 µA), and will be able to sample frequencies up to 2.5 kHz. The only such sensor we were able to find is the DRV5032, however it supports only up to 20Hz pulses.
Our questions are:
- Does TI offer any such sensor that we missed in your portfolio?
- Can the DRV5012 be manufactured in a TO-92 package, and what would be the MOQ to allow this?
Thanks,