T_ERRはT_REMOTEとは別で発生する誤差であると理解しました。
T_ERRで使用するN-factorは、N-factor Correction Registerの影響を受けますか?
適切なNファクターをRemote temp 1 η-factor correctionへ書き込めば、T_ERRは小さくなりますか?
I understand that T_ERR is a separate error from T_REMOTE.
Is the N-factor used in T_ERR affected by the N-factor Correction Register?
Will T_ERR be smaller if the appropriate N factor is written into the register "Remote temp1 η-factor correction"?
Thanks,