Other Parts Discussed in Thread: DCA1000EVM, , MMWAVEICBOOST
Hello. I am Hyunwoo Seo.
I have just purchased AWR6843ISK EVB and DCA1000EVM from TI online store, and I came up with some questions having started using it.
I would appreciate anyone who could help me with finding the answers for the following questions:
1. I read, on the document "60GHz mmWave Sensor EVMs - User's Guide", that I could capture raw data from radar EVB if used together with DCA1000.
How exactly can I capture the raw data from AWR6843ISK EVB? As I understood from the guide, I have to download a certain firmware to the board, operate it as functional mode and capture the data using DCA1000EVM. Am I getting the concept right?
2. In that case, does TI provide any pre-built example binary firmware, which I can uitilize for capturing raw data from the board?
3. Is it possible to make use of mmWave Studio with only AWR6843ISK EVB and DCA1000EVM? I cannot see clearly if mmWaveICBOOST is necessary for this application. I also have TMDSEMU11-U debug probe in hand, and I would like to know if there is any way that I can use mmWaveStudio tool without mmWaveICBOOST board.