This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112: TMP112A V.S TMP112N

Part Number: TMP112

Hi team,

If the application only need 1 % accuracy, is there any any difference using TMP112A and TMP112N?

Thanks and best regards,

Jamie

  • Hi Jamie,

    If they are operating at 3.3V and assuming your limit is either +/- 1ºC, or 1% of Full-Scale (from -40ºC, to 125ºC). I would say no, there is no difference if they don't care about the additional accuracy provided by the A version in that narrower temperature range (0 ºC, to 65 ºC)

    Best Regards,
    Brandon Fisher