Other Parts Discussed in Thread: MSP-EXP430F5529LP, TUSS4470, TDC1000, TDC1000-Q1, BOOSTXL-TUSS4470
3. Is it possible to connect the TUSS4470 with a transducer above 1Mhz?
6. Do we have to connect two transducers in TDC1000-C2000EVM ? Is it working well with one transducer?
7. What is the uVrms (min.) of the received ultrasonic signal in TDC1000 or TDC1000-Q1 ?
8. What is the maximum Fout(tx) that TDC1000 or TDC1000-Q1 still working well? Fout(tx)typ. is written 4Mhz.
9. Is the power supply up to 5.5V in TDC1000 will cause less performance regarding the received ultrasonic data, in a comparison with TUSS4470 that its power supply is up to 36V?