Other Parts Discussed in Thread: LDC2114, , LDC3114-Q1, LDC3114
Hi,
I bought an EVM for the LDC2114 but unfortunately, I cannot configure the device without breaking the GUIs functionality.
- If I start the GUI and directly switch into data streaming (and press start streaming), everything works as expected
- If I switch to configuration, modify something and switch to data streaming, start streaming does nothing, also registers view shows 0x00 for every register then
- If I switch to registers view, i can read registers but if i modify one and reread registers, the initial configuration is restored automagically
GUI Version: 1.10.0
Firmware of the LDC EVM is updated to the latest version
Any advice? It seems, that switching to configure tab will completely break communication with the EVM and write of registers does not work at all
Thanks in advance,
Martin