Hi,
Customer wants to use multiple radars for data collection, but does not know if there are interference problems with multiple radars?
if radar can be set to receive only so that it can only receive the waves emitted by other radars?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer wants to use multiple radars for data collection, but does not know if there are interference problems with multiple radars?
if radar can be set to receive only so that it can only receive the waves emitted by other radars?
Yes, radar can be easily programmed to receive only. The only change you need is: do not enable any of the TX in the chirp configuration.
Best,
Zigang
I would suggest you to change it directly from configuration file. You can modify your chirp configuration lines from:
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
and Modified to
chirpCfg 0 0 0 0 0 0 0 0
chirpCfg 1 1 0 0 0 0 0 0
chirpCfg 2 2 0 0 0 0 0 0
To disable all the TX channel.
Best,
Zigang