This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Ethernet Connection Doesn't Work

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843

My setup consists of an IWR6843 ISK-ODS interfaced with DCA100EVM to capture raw data. I am facing the following issue.

On the 'SensorConfig' tab inside mmWave Studio, when I select 'SetUp DCA1000' and then click 'Connect, Reset and Configure', nothing happens. It seems like the ethernet connection is not working. Below I have attached (i) pictures of my setup, (ii) screenshots of mmWave studio sofware, (iii) screenshot of ethernet connection settings, and (iv) mmWave Studio output.

I would appreciate if someone can help me resolve this issue.

[20:53:57]  ***Script completed successfully.***
[20:54:02]  [RadarAPI]: Opening Gpio Control Port()
[20:54:02]  [RadarAPI]: Status: Passed
[20:54:02]  [RadarAPI]: Opening Board Control Port()
[20:54:02]  [RadarAPI]: Status: Passed
[20:54:03]  [RadarAPI]: ar1.FullReset()
[20:54:03]  [RadarAPI]: Status: Passed
[20:54:04]  [RadarAPI]: Closing Board Control Port()
[20:54:04]  [RadarAPI]: Status: Passed
[20:54:04]  [RadarAPI]: Closing Gpio Control Port()
[20:54:04]  [RadarAPI]: Status: Passed
[20:54:04]  [RadarAPI]: ar1.SOPControl(2)
[20:54:04]  [RadarAPI]: Status: Passed
[20:54:05]  [RadarAPI]: ar1.Connect(16,115200,1000)
[20:54:06]  [RadarAPI]: ar1.Calling_IsConnected()
[20:54:07]  [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[20:54:07]  [RadarAPI]: Status: Passed
[20:54:07]  [RadarAPI]: ar1.frequencyBandSelection("60G")
[20:54:07]  [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[20:54:07]  [RadarAPI]: Status: Passed
[20:54:07]  Device Status : IWR6843/QM/SOP:2/ES:2
[20:54:07]  [RadarAPI]: ar1.SaveSettings('C:\Users\Usman\AppData\Roaming\RSTD\ar1gui.ini')
[20:54:10]  [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\radarss\\xwr68xx_radarss.bin")
[20:54:10]  [RadarAPI]: Downloading BSS ROM RPRC Binary..
[20:54:58]  [RadarAPI]: ar1.GetBSSFwVersion()
[20:54:58]  [RadarAPI]: BSSFwVersion:(06.02.01.05 (09/03/20))
[20:55:02]  [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\masterss\\xwr68xx_masterss.bin")
[20:55:02]  [RadarAPI]: Downloading MSS RPRC Binary..
[20:55:21]  [RadarAPI]: ar1.GetMSSFwVersion()
[20:55:21]  [RadarAPI]: MSSFwVersion:(02.00.00.03 (27/08/19))
[20:55:22]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[20:55:22]  [RadarAPI]: Status: Passed
[20:55:23]  MSS power up done async event received!
[20:55:24]  [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[20:55:24]  [RadarAPI]: Status: Passed
[20:55:24]  [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[20:55:24]  [RadarAPI]: Status: Passed
[20:55:24]  Device Status : IWR6843/QM/SOP:2/ES:2
[20:55:24]  [RadarAPI]: ar1.RfEnable()
[20:55:24]  BSS power up done async event received!
[20:55:24]  [RadarAPI]: Status: Passed
[20:55:25]  [RadarAPI]: ar1.GetMSSFwVersion()
[20:55:25]  [RadarAPI]: MSSFwVersion:(02.00.00.03 (27/08/19))
[20:55:25]  [RadarAPI]: ar1.GetBSSFwVersion()
[20:55:25]  [RadarAPI]: BSSFwVersion:(06.02.01.05 (09/03/20))
[20:55:33]  [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[20:55:33]  [RadarAPI]: Status: Passed
[20:55:34]  [RadarAPI]: ar1.LPModConfig(0, 0)
[20:55:34]  [RadarAPI]: Status: Passed
[20:55:35]  [RadarAPI]: ar1.RfInit()
[20:55:35]  RF Init async event received!
[20:55:35]  [RadarAPI]: Status: Passed
[20:55:35]  [RadarAPI]: Time stamp, Temperture: 10678,44; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 1, 1; RxIQMM Status, Update: 1, 1; 
[20:55:38]  [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
[20:55:38]  [RadarAPI]: Status: Passed
[20:55:39]  [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[20:55:39]  [RadarAPI]: Status: Passed
[20:55:40]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
[20:55:40]  [RadarAPI]: Status: Passed
[20:55:44]  [RadarAPI]: ar1.ProfileConfig(0, 60, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 131072, 30)
[20:55:44]  [RadarAPI]: Status: Passed
[20:55:45]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0)
[20:55:45]  [RadarAPI]: Status: Passed
[20:55:46]  Test Source Already Disabled...!!!
[20:55:46]  [RadarAPI]: ar1.DisableTestSource(0)
[20:55:46]  [RadarAPI]: Status: Passed
[20:55:46]  [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1)
[20:55:46]  [RadarAPI]: Status: Passed
[20:55:48]  [RadarAPI]: ar1.GetCaptureCardDllVersion()
[20:55:48]  [RadarAPI]: Sending dll_version command to DCA1000
[20:55:48]  [RadarAPI]: 
[20:55:48]  DLL Version : 1.0
[20:55:48]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[20:55:48]  [RadarAPI]: Status: Passed
[20:55:50]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[20:55:50]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
[20:55:50]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[20:55:51]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[20:55:51]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
[20:55:51]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[20:55:53]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[20:55:53]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
[20:55:53]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)