Other Parts Discussed in Thread: IWR1843, IWR1443, TIDEP-0091, IWR1443BOOST,
Hi Dear
I am using IWR1843 and MSP432P401R.
I read this file "Fluid-level sensing using 77-GHz millimeter wave" which used IWR1443 sensors and MSP.
I connect IWR1843 and MSP432P401R with 20 pin port
now I have some qustons:
1- Can I use IWR1843 instead of IWR1443?
2- Do you have examole code for this application (Link)?
3- Should I do some change in configuration of radar for work?
Best Regards
Hadi