Other Parts Discussed in Thread: AWR2243, , DCA1000EVM, AWR1843BOOST, AWR1843, AWR1243
I am interested on the chip AWR2243 and i would like to buy AWR2243BOOST evaluation board + the DCA1000EVM for real time evaluation.
I have checked the web and the related pdf´s but i could not really understand what are the outputs i will get as soon as i connect the system to a host pc. Specific questions such as the type of signal (or information) i will get and how i can work with it.
Another important question is if it is possible to work in a linux environment at low level, i see that in the manuals make reference to "MMWAVE-STUDIO-2G – with a web browser but Can i work with the signals (i.e. the range profile) at low level, such as python or c++?